METHOD GetMonthShort : CharBufferPtr
returns the localized text of the month as short name. If no localization exists, a defaulttext (textid) should be returned. The stored value, the returnpointer is set to, will be overridden by any next call of one of the Get-methods of this functionblock. Therefore, the result should be used at once. The pointer should not be stored.
InOut: |
|