METHOD StartOperation : SysTypes.RTS_IEC_RESULT
This method will be called when a read or write operation on the current instance operation is started. The return value can either be:
ERR_OK: operation successfully started
any other error code: starting an operation is not possible (at the moment)
InOut: |
|