VisuStructSimpleRectWithBorder (STRUCT)

TYPE VisuStructSimpleRectWithBorder EXTENDS VisuStructSimpleRectangle : STRUCT

InOut:

Name

Type

Comment

Inherited from

ptTopLeft

VisuStructPoint

this structure only contains the topleft and the bottomright point of a rectangle it is used if the other points don’t contain information and space is expensive ;) setter and getter for the single member: as we want to have access within the AP, we prefer single properties. See IVisuStructSimpleRectangle2

VisuStructSimpleRectangle

ptBottomRight

VisuStructPoint

setter and getter for the single member: as we want to have access within the AP, we prefer single properties. See IVisuStructSimpleRectangle2

VisuStructSimpleRectangle

iBorderWidth

INT

xScaleBorder

BOOL