FUNCTION_BLOCK Delete EXTENDS CBM.ETrig
This function block deletes a file.
Contrary to the original CAA specification the file may be deleted even if it is opened via ”FILE.Open”.
This behavior is dependent of the underlying operating system and file system.
InOut:
|
Scope
|
Name
|
Type
|
Comment
|
Inherited from
|
Input
|
xExecute
|
BOOL
|
Rising edge: Action starts
Falling edge: Resets outputs
If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.
|
ETrig
|
Output
|
xDone
|
BOOL
|
TRUE: Action successfully completed
|
ETrig
|
xBusy
|
BOOL
|
TRUE: Function block active
|
ETrig
|
xError
|
BOOL
|
TRUE: Error occurred, function block aborts action
FALSE: No error
|
ETrig
|
Input
|
sFileName
|
CAA.FILENAME
|
Name of the file to be deleted
|
|
Output
|
eError
|
ERROR
|
Local library error ID (0: no error; 5101: time out)
|
|
|