DirList (FB; Prefix fildls)

FUNCTION_BLOCK DirList EXTENDS CBM.ETrig

This function reads directory entries. The function block needs a valid handle which identifies the directory as a transfer parameter. The information is written to structure ”deDirEntry” of type ”FILE_DIR_ENTRY”. If the function block cannot find any further entries the error message ”ERROR.NO_MORE_ENTRIES” is generated and the entries in the structure ”deDirEntry” are deleted.

InOut:

Scope

Name

Type

Comment

Inherited from

Input

xExecute

BOOL

Rising edge: Action starts

Falling edge: Resets outputs

If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.

ETrig

Output

xDone

BOOL

TRUE: Action successfully completed

ETrig

xBusy

BOOL

TRUE: Function block active

ETrig

xError

BOOL

TRUE: Error occurred, function block aborts action

FALSE: No error

ETrig

Input

hDir

CAA.HANDLE

Directory handle

Output

eError

ERROR

Local library error ID (5106 - FILE_NO_MORE_ENTRIES: no further entries available)

deDirEntry

FILE_DIR_ENTRY

Directory entry