Close (FB)

FUNCTION_BLOCK Close EXTENDS CBM.ETrig

Close a serial com port opened via the FB COM.Open. The output handle hCom must be used here to close the COM port!

InOut:

Scope

Name

Type

Comment

Inherited from

Input

xExecute

BOOL

Rising edge: Action starts

Falling edge: Resets outputs

If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.

ETrig

Output

xDone

BOOL

TRUE: Action successfully completed

ETrig

xBusy

BOOL

TRUE: Function block active

ETrig

xError

BOOL

TRUE: Error occurred, function block aborts action

FALSE: No error

ETrig

Input

hCom

CAA.HANDLE

Handle to the open COM port. Ist returned by the COM.Open function block.

Output

eError

ERROR

Local library error ID (0: no error; 5001: time out)