Command: Commit, Commit project

Symbol:

Function: The command commits changes that were made in CODESYS to the SVN repository. The Commit dialog opens for this purpose.

Call:

Requirement: At least one object has been modified. An object whose contents have been modified is overlaid in the object tree with the , , or symbol.

When you execute the command, the lock on the objects to be committed is lifted automatically.