Symbol:
Function: The command opens a tab that shows the result of the comparison of your working copy and the HEAD revision. The HEAD revision is the top-level revision in the branch. You can revert specific changes that were committed to the HEAD revision.
Call: Context menu: SVN
Requirement: The object is versioned and not conflicted.
Multiple tabs can be open at the same time with the comparison of different objects.
Comparison by object type
The comparison dialog makes use of the functionality of the Project → Compare command in CODESYS. As a result, objects are compared according to their object type.