Command: SVN Repository Browser

Symbol:

Function: The command opens the SVN repository browser. The contents of an SVN repository is displayed in a tree structure here. You can search through the repository in the browser.

Call: Project → SVN menu

Depending on the selected object, the following commands are available in the context menu:

Double-clicking the object with the right mouse button opens the log dialog.