Command: Work in Offline Mode

Function: The command switches to SVN offline mode. In SVN offline mode, the implicit locking and all commands which access the SVN repository are not possible.

Call:

Requirement: The project is linked to SVN.

When switching back to SVN online mode, all existing locks on the working copy are checked against the server. If the lock is invalid, then it is released.