Command: Read Cam Online File

Function: The command reads an external file with cam data. The file extension is CAM. The cam is displayed in the cam editor.

Call: Cam menu

Requirement: The cam editor is open.

The Write Cam Online File command creates an appropriate file in CAM format.