Visualizing Alarm Management

You can use the Alarm Table and Alarm Banner visualization elements to create a display and user interface for the alarm management of an application. The alarm table lists the alarms. The alarm banner is a simplified version of the alarm table. It visualizes a single alarm only. However, by adding scroll elements to the banner you can allow for switching the display from one active alarm to another active alarm.

You can specify the optical representation of the alarms in the visualization in the display settings of an alarm class. As a result, alarms of different alarm classes can be clearly separated from each other optically.