Command: HMI Views

Function: This is a list of all views that help you as an HMI developer for creating an HMI application: Data Sources, HMI Features, Programming, and Visualizations.

Call: View menu

Requirement: The command is visible when HMI is displayed in the programming system.

An HMI project can contain any number of applications for both controllers and HMI devices. However, a view contains only the objects that are linked into the selected application.

This application is selected in the list box List of all applications. The list is located in the standard toolbar. It lists all applications of the project and always the POUs entry. When the POUs entry is selected, the objects valid across the project are displayed in the views (similar to the POUs view).