Function: The command opens the Move to Position dialog to input another position number within the Tab Order that is defined in the Command: Visualization Element List. Multiple elements can be selected for this as long as they do not belong to different groups (different hierarchy levels).
Call: Element list in the visualization editor; context menu in the Tab Order column