Symbol:
Function: The command opens the Visualization Element Repository dialog opens for editing the location and visualization profile.
Call: Tools menu
Requirement: No project is open.
Repository to manage the visualization profiles and the visualization element libraries
If you want to use your own control, you have the following options:
Integrate the control as an HTML5 control
Use the control in a frame
You can configure and use the frame like a visualization element.
For more information, see: