Function: The dialog defines the permissions of user groups for a visualization element.
Call: Click in the Value field of the Access rights element property of a visualization element.
Requirement: A visualization element is selected in a visualization and the Properties view is open.
User groups |
Groups which were configured in the Visualization Manager on the User Management → Groups tab |
Operational |
|
Only visible |
|
Invisible |
|
Group hierarchy is used |
Display whether the option Use group hierarchy is activated in the Visualization Manager on the User Management → Settings tab. A group which is of a higher hierarchy cannot have fewer permissions for an element than an element of a lower hierarchy. |
If no user is logged in, then the permissions apply for the visualization elements that are configured for the user group None. If the permissions for a visualization element is restricted, then the group None should be granted the lowest permissions.