Function: The dialog is part of the wizard that opens when you create a new project with the HMI project template. This allows for adding usual objects conveniently.
Call: Automatically after the Create HMI Project – Connect to HMI Device dialog
Alarm Configuration |
|
Image Pool |
|
Recipe Manager |
|
Text List |
|
Unit Conversion |
|
Trend Recording Manager |
|
Program |
|
Next |
Takes over the selection and opens the Create HMI Project – Choose Perspective dialog |
Abort |
Applies the configuration and creates an HMI project |