The following describes those style entries which you as a user need to know in order to influence the appearance of the visualization or elements.
A visualization style can basically be edited with the Visualization Style Editor. You can call the editor in the Visualization Manager. If a style is preset there, then you can open the editor with that style to create a new style (derived from it). From our point of view, this is the easiest way to create your own visualization style.
Continue as follows:
Select a visualization style which is closest to what you want.
Use the command icon to toggle the insert mode.
The insert mode on the Style Properties tab is set to flat.
When the insert mode is set to flat, you can apply the style entry names from the following tables.