Setting Up Multiple Languages

Texts and tooltip texts for visualizations are managed in text lists and can be displayed in different languages. To toggle a visualization between the available languages, configure a visualization element with the corresponding input configuration for "changing the language".

There are static texts that are managed in GlobalTextList (generated automatically) and dynamic texts from created text lists. A dynamic text can be changed at runtime with a variable that defines the index of the text list entry. Static texts are fixed labels within a visualization; dynamic texts are often used for displaying variable values or error messages.

For creating and using text lists, see: ../../..//index.htm.

TIP:

You can modify the appearance and formatting of texts and tooltips with the element properties Text properties and Font variables.

NOTE:

For Unicode strings to be displayed, you have to enable the Use Unicode strings setting on the Settings tab of the Visualization Manager.