IActionController2.ControlSampleAction (METH)

METHOD ControlSampleAction

An action controller is used whenever it is necessary to have the actions of the action controller instead of those of the action provider called. ControlSampleAction is the action controller specifically used to control the first invocation of the STATE.STARTING state.

InOut:

Scope

Name

Type

Input

itfSampleActionProvider

ISampleActionProvider

Output

iErrorID

INT