METHOD StartAction
The StartAction is running until either the output xComplete is TRUE or iErrorID ≠ 0 (Zero). If xComplete is TRUE the state STATE.EXECUTING is reached. If there is a iErrorID ≠ 0 (Zero) the state STATE.CLEANING is reached.
To sample the inputs in the first invocation of a function block the method SampleAction is the solution of choice. See: ISampleActionProvider.SampleAction
InOut: |
|