METHOD GetAlreadyExistingRecipes : BOOL
This method is called at the start of an application and checks all currently existing recipe files so they can be reused if so configured.
Scope
Name
Type
Return
GetAlreadyExistingRecipes
BOOL