RecipeManCommands.LoadRecipe (METH)

METHOD LoadRecipe : DWORD

Loads a recipe from the standard recipe file

The standard recipe file name is <recipe>.<recipedefinition>.<recipeextension>.

Note

Entries in the recipe that do not include value assignments are not loaded and written. Refer to the “Load and write Recipe” command.

InOut:

Scope

Name

Type

Comment

Return

LoadRecipe

DWORD

Possible last error values:

See ReturnValues (GVL) for a description of all possible errors.

Input

RecipeDefinitionName

STRING

Name of the recipe definition

RecipeName

STRING

Name of the recipe