class
IScriptTestSetObject.
IScriptTestSetObject
Bases: object
Class provides methods to manipulate test set objects.
test_data_type_name
Retrieves or sets the data type (DUT) used the definition of test runs.
string
test_runs
Retrieves a sequence of the test runs defined in this IScriptTestSetObject . Internally, the test run is referenced by its index. Therefore, the returned reference is only valid, as as long as the index of the test run has not changed.
List of IScriptTestRun