Inout
|
ncprogIn
|
SMC_CNC_REF
|
|
CNC program input
|
Input
|
bExecute
|
BOOL
|
|
Rising edge starts operation.
|
pBuffer
|
POINTER TO SMC_GCODE_WORD
|
|
Memory for internal buffer
|
dwBufferSize
|
UDINT
|
|
Size of pBuffer
|
pBufferOut
|
POINTER TO SMC_GCODE_WORD
|
|
Memory for ncprogOut
|
dwBufferOutSize
|
UDINT
|
|
Size of pBufferOut in byte
|
historyBuffer
|
SMC_ISentenceHistory
|
|
A function block keeping track of all G-Code sentence numbers that have been processed and removed from the jump buffer. If no buffer is provided, the default implementation SMC_MonotoneSentenceHistory will be used.
|
udiRefillWindowSizePercentage
|
UDINT
|
10
|
The amount of elements that is read and removed in one cycle and added in the next cycle, when no jump has been requested (if ncprogOut.bRestart=FALSE). Provided in percent of the current buffer level and defaults to a minimum value of 10. A larger center window will slightly improve reading performance for long cycle times, while reducing the buffer’s chances to have a requested jump target actually buffered.
|
Output
|
bBusy
|
BOOL
|
|
|
bDone
|
BOOL
|
|
|
bError
|
BOOL
|
|
|
ErrorID
|
SMC_ERROR
|
|
|
ncprogOut
|
SMC_CNC_REF
|
|
CNC program output to SMC_NCDecoder
|
bExecuteDecoder
|
BOOL
|
|
Set to TRUE as soon as ncprogOut is filled sufficiently to be interpreted by SMC_NCDecoder;
|