TP (FB)

FUNCTION_BLOCK TP

Implements a pulse timer

(* Example declaration *)
TPInst : TP ;

(* Example in ST *)
TPInst(IN := VarBOOL1, PT:= T#5s);
VarBOOL2 := TPInst.Q;
InOut:

Scope

Name

Type

Comment

Input

IN

BOOL

Rising edge starts the pulse timer and sets Q to TRUE

PT

TIME

Length of the pulse (high-signal)

Output

Q

BOOL

Pulse signal, set to TRUE for PT milliseconds if EN has a rising edge

ET

TIME

Elapsed time since pulse timer started. It will then remain constant after PT is reached.