CharBufferString.Copy (METH)

METHOD Copy : DINT

Does a strcpy from the source string cbsSource into our instance. Will return the number of copied characters including the terminating ‘0’ or “0”

InOut:

Scope

Name

Type

Return

Copy

DINT

Input

cbsSource

REFERENCE TO CharBufferString