FUNCTION StrPadRightA : BOOL
This function generate a padding string and concatenates it with pstFrom to pstTo if the iBufferSize from pstTo is big enough. The function will do its work either with native IEC-Strings or with strings coming from external functions. It will return FALSE and does no concatenation if one of the strings is NULL or the buffer size is not big enough.
InOut: |
|