Util Library Documentation

Company

System

Title

Util

Version

3.5.19.0

Categories

Application|Common

Author

3S - Smart Software Solutions GmbH

Placeholder

Util

Description [1]

Provides data types for generator modes and points. And provides function blocks and functions for the following use cases: Analog monitors, BCD conversions, bit/byte functions, controller, function manipulators, mathematical functions and signals.

In the folder TimerSwitch the types, functions and function blocks are located for handling UTC and local time and the implementation of a timer switch.

Contents:

Indices and tables

[1]

Based on Util.library, last modified 02.03.2023, 10:46:37. LibDoc 4.0.0.0

The content file Util.clean.json was generated with CODESYS V3.5 SP16 Patch 3 on 02.03.2023, 10:46:40.