Input
|
xEnable
|
BOOL
|
|
TRUE: Activates the defined operation FALSE: Aborts/resets the defined operation
|
LConC
|
Output
|
xBusy
|
BOOL
|
|
TRUE: Operation is running
|
LConC
|
xError
|
BOOL
|
|
TRUE: Error condition reached
|
LConC
|
Input
|
itfDateTimeProvider
|
IDateTimeProvider
|
Globals.g_dtpDateTimeProvider
|
Source for the current date and time information in milliseconds since 1.1.1970 00:00:00.000
|
|
tCompensationSpeed
|
TIME
|
|
Compensation speed [ms/h] for the transition from one time zone period to another.
e.g. t#5000ms => 30d <= 1/(30 × 24) × 60 × 60 × 1000
e.g. t#150000ms => 24h <= 1/24 × 60 × 60 × 1000
|
|
aslSchedule
|
POINTER TO Schedule
|
|
Switching Schedule
|
|
tzTimeZone
|
REFERENCE TO TimeZone
|
|
Current time zone (Optional - Default:
|gc_tzTimeZoneCET|)
|
|
Output
|
eErrorID
|
ERROR
|
|
|
|
liClockDiff
|
LINT
|
|
After switching the time zone, a continuously decreasing difference between the current local time and the current time within the TimeSwitch is displayed.
|
|
eWeekDay
|
WEEKDAY
|
|
Current day of the week
|
|
datToday
|
DATE
|
|
Current date
|
|
todNow
|
TOD
|
|
Current time of the day
|
|
sTimeZone
|
TZ_NAME
|
|
Name of the current time zone
|
|
ePeriod
|
PERIOD
|
|
Current period of the time zone
|
|
dwSwitches
|
DWORD
|
|
Status of the 32 switches. Bit 0 => switch 1, …
|
|