This method searches for a style entry of type UDINT and returns the according value if found.
InOut:
Scope
Name
Type
Comment
Return
GetUDINT
UDINT
Input
stStyleKey
STRING
The name of the style entry to seach for.
udiDefault
UDINT
The default value to use if the entry is not found.
pOptResult
POINTER TO UDINT
An optional result error code. Common result values are Errors.ERR_OK if a valid style was found or Errors.ERR_INVALIDID if no style entry was found. In this case, the method will return the default value.