INTERFACE IVisuStreamReader EXTENDS IVisuStreamHandler
Implementors of this interface can be configured in the input action “File Transfer” in case of streaming data from the plc to the visualization
Methods:
EndOperation, inherited from IVisuStreamHandler
StartOperation, inherited from IVisuStreamHandler
Structure: