VisuFctGetAbsolutePosition (FUN)

FUNCTION VisuFctGetAbsolutePosition : VisuStructSimpleRectangle

Returns the absolute position of a visual element in overlay mode. If the element is rotated the result is the surrounding rect.

InOut:

Scope

Name

Type

Return

VisuFctGetAbsolutePosition

VisuStructSimpleRectangle

Input

itfVisualElement

IVisualElement

itfClientObjectInfo

IClientObjectInfo

pSelectionRect

POINTER TO VisuStructSimpleRectangle

Inout

clientData

VisuStructClientData