|
(ANY_TO_INT(60) * ANY_TO_INT(2))
|
The length of the STRING representing the placeholder value used for the placeholder replacement in the functions ReplaceAlarmPlaceholders4 and ReplaceAlarmPlaceholders3. If WSTRING is used this parameter represents the number of bytes. Example: If the maximum length of a WSTRING to format is 90, this parameter must be set to 2 * (90 + 1) = 182
|