FUNCTION AlarmStorageGetDefaultText : CharBufferPtr
This function can be used to determine the default text of a message of an alarm, that was read from the alarm storage.
|
InOut:
|
|
Scope
|
Name
|
Type
|
Comment
|
|
Return
|
AlarmStorageGetDefaultText
|
CharBufferPtr
|
A CharBufferPtr containing the default text. A NULL pointer if the corresponding information cannot be retrieved
|
|
Input
|
udiAlarmGroupId
|
UDINT
|
The internal id of the alarm group, that was read from the alarm storage
|
|
udiAlarmId
|
UDINT
|
The internal id of the alarm, that was read from the alarm storage
|
|
iWhichMessage
|
INT
|
The 1-based index of the text id.
|
|
stringType
|
__SYSTEM.TYPE_CLASS
|
A __SYSTEM.TYPE_CLASS indicating, which type of string has to be retrieved. Pass either __SYSTEM.TYPE_CLASS.TYPE_STRING or __SYSTEM.TYPE_CLASS.TYPE_WSTRING
|
|