This tab contains the basic settings for network communication.
Watchdog |
The incoming data (holding registers / %I range) is set to zero when the Modbus device does not receive any valid query from the master. |
Closing the TCP socket |
|
Slave port |
Port number of the slave |
Bind to Adapter |
This option is relevant for systems with multiple Ethernet adapters.
|
Holding registers (%IW) |
Number of holding registers: possible values: 1–4096. The maximum number can be limited in the device description.
Writable: |
Input registers (%QW) |
Number of input registers: possible values: 1–4096. The maximum number can be limited in the device description. |
Discrete Bit Areas |
The Modbus coils and discrete inputs get their own data area. By default, the register access and bit access use the same Modbus data. |
Coils |
Number of Modbus coils |
Discrete inputs |
Number of Modbus discrete inputs |
Changes to the input/output assembly size have a direct effect on the number of configurable parameters in the I/O mapping.
Modbus defines for I/O data a data model with four areas.
Inputs and outputs are included as with all fieldbuses, but from the point of view of the "host". These data areas have any number of logical start offsets as defined by the manufacturer. The I/O data behind the Modbus data areas can overlap or be independent of each other. For details about the Modbus data model, see Modbus Protocol Specification in Chapters 4.3 and 4.4 (www.modbus.org). In the case of the CODESYS Modbus Device, the input registers and discrete inputs, as well as the holding registers and coils, are all mapped to the same I/O data. This is also the case when they are addressed via different logical start offsets. |
|
Coils |
Definition of the start address of the respective Modbus data area |
Discrete inputs |
|
Holding register |
|
Input register |
|
Holding and input register data areas overlay |
This is required, for example, when the slave application is used to write to the holding register. |