The parameters of the PROFIBUS Slave are defined on this tab. The parameters are defined in the device description file, but they can be edited in this dialog.
Station Address |
Permitted range from 0 to 126. Every new device inserted into the bus is assigned an incremented address automatically. Note: Address 126 is the default DP Slave address. Addresses are checked for duplicates. |
ID number |
Unique number that was assigned to this device type from the PNO. This allows a unique reference between the DP Slave and the GSD file. |
TSDR (Tbit): |
"Time Station Delay Responder". Earliest response time that the slave can respond to the master (min. 11 Tbit) |
Lock/Unlock: |
The slave is blocked or released for other masters
|
* TBit: Time unit for transmission of a bit via PROFIBUS; reciprocal value of the transmission rate; e.g. 1 Tbit at 12MBaud = 1/12,000,000 bps=83ns
Watchdog control: |
|
Time (ms): Monitoring time, relevant to the case when the "Watchdog control" option is active. |
Monitoring time, relevant to the case when the Watchdog control option is active. |
Groups |
Opens the Groups dialog. |
In addition to the base DP parameters, user parameters are the individual parameters of a DP Slave. When they are defined in the device description file (GSD file), they are displayed here. The parameter values can be edited by clicking the corresponding field in the Value column. |
|
Symbolic values |
|
Length of the user parameters (Byte) |
Added user parameters that are defined by the device description file. |
Defaults |
Returns the values to the default settings. |