Symbol:
Function: The command aligns the selected visualization elements in a line through the top edge of the element positioned furthest up.
Call: Visualization → Alignment menu; context menu
Requirement: Multiple elements are selected.