Command: Choose Perspective

Function: The command lets you switch between the CODESYS perspective and the HMI perspective.

Call: View menu.

CODESYS Perspective

CODESYS is displayed in the usual tree oriented perspective in which IEC applications are typically developed.

HMI Perspective

CODESYS is displayed in the HMI perspective that supports the development of HMI applications.

The perspective is subdivided into individual views: Visualizations, Data Sources, and HMI Features.