Hoisting Position Synchronization

 

Overview

This part explains the functionality and implementation of HoistPositionSync function block in the Hoisting Library.

What Is in This Part?

This part contains the following chapters:

oHoistPositionSync_2: Position Synchronization of Two Crane Axes