3S - Smart Software Solutions GmbH
IoDrvCIFXProfibus
4.1.0.0
Intern|IoDrivers
IoDrvCIFXProfibusLibrary
IoDrvProfibusMaster
IO Driver Profibus for Hilscher netX chip.
CommFB
PB_CNCT (FunctionBlock)
Constants
NetXErrorCodes (GVL)
Diag
IoDrvCIFXProfibusDiag (FunctionBlock)
PBSlaveDiag (FunctionBlock)
ProfibusBaudrate (Enum)
FunctionBlocks
CommunicationErrorCIFX (Enum)
IoDrvCIFXProfibus (FunctionBlock)
PBSlave (FunctionBlock)
RedundancyStatus (FunctionBlock)
[1]
Based on IoDrvCIFXProfibus.library, last modified 23.05.2023, 08:33:12. LibDoc 4.0.0.0
The content file IoDrvCIFXProfibus.clean.json was generated with CODESYS V3.5 SP16 Patch 3 on 23.05.2023, 08:33:12.