FUNCTION_BLOCK ControllerConfigUtil
This function block can be used to adapt some parameters of the initially downloaded profinet controller config-structure (device tree).
For example this way the IP-adresses of the slaves that are configured for this controller can be adapted at runtime.
The FB is typically used with the Reconfigure-feature (see DED.Reconfigure function block).
Example: Reconfigure a single slave
PROGRAM PLC_PRG
VAR
ip : ProfinetCommon.IPParameterValue := (IPAddress := [192, 168, 0, 2], Subnetmask := [255, 255, 255, 0]);
i : DINT;
enable : BOOL := FALSE;
moduleDevice : DED.IDevice;
reconf : DED.Reconfigure;
configUtil : IoDrvProfinetBase.ControllerConfigUtil;
updateIP : IoDrvProfinetBase.ConfigError;
END_VAR
//note: pn_device is some (initially disabled) profinet slave in the device-tree of the application
IF(enable AND NOT pn_device.Enable) THEN
updateIP := configUtil.UpdateIPSettings(pn_device, ip); // change configured ip-address
//enable device and modules
pn_device.Enable := enable;
FOR i := 0 TO TO_DINT(pn_device.ChildNodeCount) - 1 DO
moduleDevice := INode_To_IDevice(pn_device.GetChild(TO_UDINT(i)));
configUtil.UpdateSlotNumber(moduleDevice, TO_UINT(i + 1)); // change configured slot number
moduleDevice.Enable := enable;
END_FOR
reconf.xExecute := TRUE;
END_IF
reconf(itfNode := pn_device); //start reconfigure
Methods:
Structure: