IF_RobotTSeries - SetDigitalTwinConfigData (Method)

Overview

Type:

Method

Available as of:

V2.14.0.0

Versions:

Current version

This chapter provides information on:

Task

Set the configuration data for the EcoStruxure Machine Expert Twin communication of the Lexium T Robot.

Description

By calling the method, the provided configuration data are verified, stored, and transferred into the OPC UA data structure of the Lexium T Robot.

Interface

Input

Data type

Description

i_stData

DTC.ST_ConfigDataRobotTSeries

Configuration data for EcoStruxure Machine Expert Twin.

NOTE: i_stData.sCategory and i_stData. xParallelLinkageLeft are overwritten by the value stored inside the function block.

i_udiArrayIndex

UDINT

The array index number indicates the robot related OPC UA data structure, for example, DTC.GVL_OpcUaRobotics.G_stROB.astRobotTPSeries[i_udiArrayIndex].

Output

Data type

Description

q_etDiag

GD.ET_Diag

General, library-independent statement on the diagnostic.

A value not equal to ET_Diag.Ok corresponds to a diagnostic message.

q_etDiagExt

ET_DiagExt

POU-specific output for the diagnostic.

q_etDiag = ET_Diag.Ok -> Status message

q_etDiag <> ET_Diag.Ok -> Diagnostic message

q_sMsg

STRING[80]

Event-triggered message that gives additional information on the diagnostic state.

Diagnostic Messages

q_etDiag

q_etDiagExt

Enumeration value

Description

OK

OK

0

Successful

InputParameterInvalid

DigitalTwinNameInvalid

124

The name is invalid.

InputParameterInvalid

DigitalTwinColorInvalid

125

The color is invalid.

InputParameterInvalid

DigitalTwinUnivocalIdInvalid

126

The UnivocalID is invalid.

InputParameterInvalid

DigitalTwinArrayIndexInvalid

127

The array index is invalid.

DigitalTwinNameInvalid

Enumeration name:

DigitalTwinNameInvalid

Enumeration value:

124

Description:

The name is invalid.

Issue

Cause

Solution

Setting the EcoStruxure Machine Expert Twin configuration parameter was unsuccessful.

The configuration parameter i_stData.sName is invalid.

Verify that the configuration parameter i_stData.sName is not empty.

DigitalTwinColorInvalid

Enumeration name:

DigitalTwinColorInvalid

Enumeration value:

125

Description:

The color is invalid.

Issue

Cause

Solution

Setting the EcoStruxure Machine Expert Twin configuration parameter was unsuccessful.

The configuration parameter i_stData.udiColor is invalid.

Verify that the configuration parameter i_stData.udiColor is in the valid range of DTC.ET_EmulationColors.

DigitalTwinUnivocalIdInvalid

Enumeration name:

DigitalTwinUnivocalIdInvalid

Enumeration value:

126

Description:

The UnivocalID is invalid.

Issue

Cause

Solution

Setting the EcoStruxure Machine Expert Twin configuration parameter was unsuccessful.

The configuration parameter i_stData.udiUnivocalId is invalid.

Verify that the configuration parameter i_stData.udiUnivocalId is not 0.

DigitalTwinArrayIndexInvalid

Enumeration name:

DigitalTwinArrayIndexInvalid

Enumeration value:

128

Description:

The array index is invalid.

Issue

Cause

Solution

Setting the EcoStruxure Machine Expert Twin configuration parameter was unsuccessful.

The configuration parameter i_udiArrayIndex is invalid.

Verify that the configuration parameter i_udiArrayIndex is not 0 and i_udiArrayIndexDTC.GCL.Gc_udiMaxNumberOfRobotTSeries.