METHOD LoadFromAndWriteRecipe : DWORD
Loads a recipe from the specified recipe file and afterwards writes the recipe into the PLC variables
Entries in the recipe that do not include value assignments are not loaded and written. Refer to the “Load and write Recipe” command.
InOut: |
|