FUNCTION_BLOCK SMC_GetMParameters
If the interpolator is waiting for an M-function, this function block can be used to query the parameters that have been set for this M-function in the G-Code (K, L, O words).
|
InOut:
|
|
Scope
|
Name
|
Type
|
Comment
|
|
Inout
|
Interpolator
|
SMC_Interpolator
|
Instance of interpolator
|
|
Input
|
bEnable
|
BOOL
|
While TRUE, the function block is active
|
|
Output
|
bMActive
|
BOOL
|
The value TRUE indicates a M-function is currently active
|
|
dK
|
LREAL
|
M-parameter specified via word K
|
|
dL
|
LREAL
|
M-parameter specified via word L
|
|
MParameters
|
SMC_M_PARAMETERS
|
M-parameters, specified by a variable of type SMC_M_PARAMETERS (passed by the O-word). Example G-Code: “N00 M5 K1 L2 O$mParams$”
|
|