IVisualElementProvidesChildElements.GetElementIdArray (METH)

METHOD GetElementIdArray : POINTER TO ARRAY [0..0] OF INT

Returns a pointer to an array of the subelements’ Id’s. The number of entries is returned by the output count. If count is 0, then a return value of NULL is allowed.

InOut:

Scope

Name

Type

Return

GetElementIdArray

POINTER TO ARRAY [0..0] OF INT

Output

count

INT