METHOD GetRowHeight : INT
Returns the height of the row with the specified index.
Scope
Name
Type
Comment
Return
GetRowHeight
INT
Input
diRowIndex
DINT
The index of the row. It can be assumed that 0 <= diRowIndex < NumberOfColumns.