IDialogManager5.IsDialogOpen (METH)

METHOD IsDialogOpen : BOOL

This method checks whether a given dialog is already open

InOut:

Scope

Name

Type

Comment

Return

IsDialogOpen

BOOL

Input

pClientData

POINTER TO VisuStructClientData

A pointer to a VisuStructClientData structure identifying the client, where the check has to be done

dialog

IVisualisationDialog

The dialog to check for

Output

xModal

BOOL

whether the dialog is opened modally