IVisuStreamFileNameInfo (ITF)

INTERFACE IVisuStreamFileNameInfo

This interface can be optionally implemented by implementors of IVisuStreamReader or IVisuStreamWriter if a proposal of the filename to select should be used.

Properties:

FileNameProposal

Structure: