IDialogManager9.SetClientDataWithoutStartCycle (METH)

METHOD SetClientDataWithoutStartCycle : BOOL

this method will set the current client data in the object instance, that will be used during the following calls to Update, GetUpdateRects, Paint, HandleInput TOCHECK: removes reentrancy of objects!

InOut:

Scope

Name

Type

Return

SetClientDataWithoutStartCycle

BOOL

Input

pClientData

POINTER TO VisuStructClientData